This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2640: Error: No XDCtools are currently installed

Part Number: CC2640


Tool/software: Code Composer Studio

Hello,
I want to import CC2640 project but then an error appeared: No XDCtools are currently installed.I'm using CCS7. In the c:\ti path I found xdctools_3_32_00_06_core and xdctools_3_32_01_22_core but in the CCS Installed Software window I can't see them.

Regards, Holger

  • Holger,

    CCSv7.1 ships with 2 copies of XDCTools.  If you go to the location below in the preferences dialog (Window -> preferences) does CCS list any XDCTools?

    Really it should find the ones inside CCS as well as the ones you have in C:/ti

    You could try adding the path to each set of tools at the top of the dialog and then clicking Rediscover.  Note that after CCS finds XDCTools it does need to restart in order to be able to use them.

    Regards,

    John

  • I removed CCS7 and installed CCS7.1 and it worked now.