Hello
We have to upload the .out file to our dsp TI TMS320C64 system, as the loader inside the specific embedded OS loads the out-file directly. I am using CGT 6.1.15.
Unfortunately the .out file size increases very fast as it is a very big project. (~8MB) So I am trying to decrease the size by stripping all unnecessary information out.
strip6x -p doesn't work for me because beside the symbolic information also the necessary code for relocation is stripped out.
So I only can use strip6x without further options
In my opinion there are a lot uf useless information in the .out file which has nothing to do with my binary code:
- template symbols inside .out file:
Analyzing the .out file I saw that the templates need a very big place, as the symbols are written completely.
Is there any possibility to replace symbols with an ordering number?
- Information about environment and compiler settings:
Indeed there are information about include paths and compilersettings inside the .out file
* I already found the linker option --hide=* but there is no big effect for the codesize.
* I already stripped out debug information for compiler ( symdebug:none, no -g option)
Does anyone has solutions for me?
Thank you and best regards
Quarby