Part Number: MSP430G2744
Tool/software: TI C/C++ Compiler
CCS6.1, MSP430 compiler TI 4.3.8
Here is the piece of code:
typedef struct __attribute__((packed))
{
uint8 d0[4];
uint8 d1[2];
uint32 d2[2];
uint16 SlotInfo_Start;
uint32 EdBitmap[2];
uint16 SlotInfo_SlotNum;
ChannelIdT F0Channel;
}RfMsgDGroupEdInfoWithSlotsT;
RfMsgDGroupEdInfoWithSlotsT* groupEdInfoMsgP2 = (RfMsgDGroupEdInfoWithSlotsT*)groupEdInfoMsgP;
uint32 EdBitmap[2];
EdBitmap[0] = groupEdInfoMsgP2->EdBitmap[0];
EdBitmap[1] = groupEdInfoMsgP2->EdBitmap[1];
The compiler will generate complex code to copy EdBitmap[0] and EdBitmap[1] as following. But actually groupEdInfoMsgP2 points to an address that is 4 byte aligned in my code. Can I
specify to the compiler that groupEdInfoMsgP2 is 4 byte aligned (so member EdBitmap[2] in the structure is also 4 byte aligned), so that copying to EdBitmap[2] could be much faster?