This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: CCS. File Loader error...

Other Parts Discussed in Thread: CC2650

Tool/software: Code Composer Studio

Hello.
Yesterday there were updates. I installed them. The installation was not successful.
I can not flash the CC2650. I have the following message ....

Has made reinstallation of CCS. Did not help.
An error occurs when flashing different processors.

How can the situation be remedied?

  • Can You help me?

    .............

    And with the help of the programmer 2 it is stitched successfully.

    Moved the project. Shortened the way. Does not help.

    Deleted the Debug folder, Did a cleanup of the project. I compiled it anew.
    Did not help.

    JTAG Tested


    Do a test using 0xFFFFFFFF.
    Scan tests: 1, skipped: 0, failed: 0
    Do a test using 0x00000000.
    Scan tests: 2, skipped: 0, failed: 0
    Do a test using 0xFE03E0E2.
    Scan tests: 3, skipped: 0, failed: 0
    Do a test using 0x01FC1F1D.
    Scan tests: 4, skipped: 0, failed: 0
    Do a test using 0x5533CCAA.
    Scan tests: 5, skipped: 0, failed: 0
    Do a test using 0xAACC3355.
    Scan tests: 6, skipped: 0, failed: 0
    All of the values were scanned correctly.

    The JTAG IR Integrity scan-test has succeeded.

    -----[Perform the Integrity scan-test on the JTAG DR]------------------------

    This test will use blocks of 64 32-bit words.
    This test will be applied just once.

    Do a test using 0xFFFFFFFF.
    Scan tests: 1, skipped: 0, failed: 0
    Do a test using 0x00000000.
    Scan tests: 2, skipped: 0, failed: 0
    Do a test using 0xFE03E0E2.
    Scan tests: 3, skipped: 0, failed: 0
    Do a test using 0x01FC1F1D.
    Scan tests: 4, skipped: 0, failed: 0
    Do a test using 0x5533CCAA.
    Scan tests: 5, skipped: 0, failed: 0
    Do a test using 0xAACC3355.
    Scan tests: 6, skipped: 0, failed: 0
    All of the values were scanned correctly.

    The JTAG DR Integrity scan-test has succeeded.

    [End]

    WAU!!!!!

    Open the project properties. Select Debug. Click to set the default settings.
    The problem is solved.

  • Sergey,

    That is great that you are up and running again.  That error message comes from the flashing component in CCS.

    So you were able to flash the device using the SmartRF Flash Programmer but also had to restore defaults in the CCS program load option?  Do you recall changing any options in there?  I would like to figure out how things went wrong so that we can improve the tool or the error messages.

    Regards,

    John

  • John, good afternoon and thank you for your support.

    That day there were two events. I moved the project folder. Perhaps this project lost the settings and I used the settings of another project. Then I installed the updates. I can not say what was the update, but it was fixed with an error. I did not save the error message. Apparently the updates were not the cause of the malfunction. The problem was in the project settings as you understood.