Other Parts Discussed in Thread: CCSTUDIO
I have project that works, I installed same environment on a new laptop with Window 7 (32 bit) and now I have "segmentation fault" in some files.
I saw in previous posts a suggestion to replace the cl2000.exe with the one in:
but this did not help.
Any suggestions?
The environment is:
CCS v3.3 - 3.3.81.6
BIOS- 5.33.03
Code generation tool - v5.0.0
The error is:
INTERNAL ERROR: C:\Program Files\C2000 Code Generation Tools 5.0.0\bin\asm2000.exe experienced a segmentation fault while
processing section .text file C:/CCStudio_v3.3/MyProjects/SimplIQ2DSP/Debug/d_SpeedController.asm line 1227
This is a serious problem. Please contact Customer
Support with this message and a copy of the input file
and help us to continue to make the tools more robust.
David Y.