Tool/software: Code Composer Studio
I created a simulink model consist only of an input a unit delay and an output model and when i build it for ccs simulator it get me these two error messages.
Error 1 :
Error 2 :
Please give me a solution...
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
I created a simulink model consist only of an input a unit delay and an output model and when i build it for ccs simulator it get me these two error messages.
Error 1 :
Error 2 :
Please give me a solution...
I have no idea how this is setup - but I think you should be trying to run your simulation in Simulink and not externally via calls to the MathWokrs simulation engine (if this is indeed what you are trying to do).
Please contact MathWorks Technical Support for assistance.
-Brian
What version of MathWorks tools, CCS, and OS are you using? You may have a incompatible set-up.
I don't really understand what you are trying to do here - so I again will tell you the fastest way to get unstuck with your project to to contact MathWorks t=Tech Support.
-b
Tool/software: Code Composer Studio
-------------------------- soumya1.pjt - Custom_MW --------------------------
[MW_c6xxx_bsl.c] "D:\CCS V3.1\C6000\cgtools\bin\cl6x" -g -fr"D:/MATLAB7/work/soumya1_c6000_rtw/Custom_MW" -d"_DEBUG" -@"Custom_MW.lkf" "MW_c6xxx_bsl.c"
"D:/CCS V3.1/C6000/csl/include/csl_chiphal.h", line 262: fatal error: #error NO CHIP DEFINED (use -dCHIP_XXXX where XXXX is chip number, i.e. 6201)
1 fatal error detected in the compilation of "MW_c6xxx_bsl.c".
Compilation terminated.
>> Compilation failure
[MW_c6xxx_csl.c] "D:\CCS V3.1\C6000\cgtools\bin\cl6x" -g -fr"D:/MATLAB7/work/soumya1_c6000_rtw/Custom_MW" -d"_DEBUG" -@"Custom_MW.lkf" "MW_c6xxx_csl.c"
"D:/CCS V3.1/C6000/csl/include/csl_chiphal.h", line 262: fatal error: #error NO CHIP DEFINED (use -dCHIP_XXXX where XXXX is chip number, i.e. 6201)
1 fatal error detected in the compilation of "MW_c6xxx_csl.c".
Compilation terminated.
>> Compilation failure
[rt_nonfinite.c] "D:\CCS V3.1\C6000\cgtools\bin\cl6x" -g -fr"D:/MATLAB7/work/soumya1_c6000_rtw/Custom_MW" -d"_DEBUG" -@"Custom_MW.lkf" "rt_nonfinite.c"
"rtwtypes.h", line 12: fatal error: could not open source file "tmwtypes.h"
1 fatal error detected in the compilation of "rt_nonfinite.c".
Compilation terminated.
>> Compilation failure
[rt_sim.c] "D:\CCS V3.1\C6000\cgtools\bin\cl6x" -g -fr"D:/MATLAB7/work/soumya1_c6000_rtw/Custom_MW" -d"_DEBUG" -@"Custom_MW.lkf" "rt_sim.c"
"rt_sim.c", line 20: fatal error: could not open source file "tmwtypes.h"
1 fatal error detected in the compilation of "rt_sim.c".
Compilation terminated.
>> Compilation failure
[soumya1.c] "D:\CCS V3.1\C6000\cgtools\bin\cl6x" -g -fr"D:/MATLAB7/work/soumya1_c6000_rtw/Custom_MW" -d"_DEBUG" -@"Custom_MW.lkf" "soumya1.c"
"rtwtypes.h", line 12: fatal error: could not open source file "tmwtypes.h"
1 fatal error detected in the compilation of "soumya1.c".
Compilation terminated.
>> Compilation failure
[soumya1_main.c] "D:\CCS V3.1\C6000\cgtools\bin\cl6x" -g -fr"D:/MATLAB7/work/soumya1_c6000_rtw/Custom_MW" -d"_DEBUG" -@"Custom_MW.lkf" "soumya1_main.c"
"rtwtypes.h", line 12: fatal error: could not open source file "tmwtypes.h"
1 fatal error detected in the compilation of "soumya1_main.c".
Compilation terminated.
>> Compilation failure
[vectors.asm] "D:\CCS V3.1\C6000\cgtools\bin\cl6x" -g -fr"D:/MATLAB7/work/soumya1_c6000_rtw/Custom_MW" -d"_DEBUG" -@"Custom_MW.lkf" "vectors.asm"
Build Complete,
6 Errors, 0 Warnings, 0 Remarks.
I dont believe we support CCSv3.1. The earliest CCS we support is v3.3 (that I am aware of).
Also I think you are using MATLAB 7 - which is ancient, that was launched in June 2004, almost 13 years ago. That is 30(!!) releases ago on the MathWorks side (we are on MATLAB 9.2 currently). I don't know that you will find many technical resources available to help here - you probably need to upgrade your CCS and MathWorks tools to a much more recent release.
-Brian
I have MATLAB R2015a software....Which CCS version is supported (best combo) this matlab version..??
Check here for a compatibility chart: http://processors.wiki.ti.com/index.php/MatLab_and_CCS
-b
Now, this time i used Matlab R2012a & CCSv4.1
Please solve this matter...(point no. 2)..Does not found C6000 CSL file ??
>> xmakefilesetup
>> checkEnvSetup('ccsv4','c6713','setup')
1. Checking CCS (Code Composer Studio) version
Required version: 4.1.0
Required for : Code Generation
Your Version : 4.1.0
2. Checking C6000 CSL (TMS320C6000 Chip Support Library) version
Required version: 2.31.00.16 or later
Required for : Code generation
Warning: Installation directory for C6000 CSL is invalid.
> In C:\Program Files\MATLAB\R2012a\toolbox\idelink\extensions\ticcs\envChecker\checkEnvSetup_private.p>updateInstallDir at 519
In C:\Program Files\MATLAB\R2012a\toolbox\idelink\extensions\ticcs\envChecker\checkEnvSetup_private.p>envSetup at 277
In C:\Program Files\MATLAB\R2012a\toolbox\idelink\extensions\ticcs\envChecker\checkEnvSetup_private.p>checkEnvSetup_private at 75
In checkEnvSetup at 156
Your Version :
Warning: The folder, "", required to set environment variable CSL_C6000_INSTALLDIR does not
exist. Check your installation.
> In C:\Program Files\MATLAB\R2012a\toolbox\idelink\extensions\ticcs\envChecker\checkEnvSetup_private.p>setEnvVar at 584
In C:\Program Files\MATLAB\R2012a\toolbox\idelink\extensions\ticcs\envChecker\checkEnvSetup_private.p>envSetup at 321
In C:\Program Files\MATLAB\R2012a\toolbox\idelink\extensions\ticcs\envChecker\checkEnvSetup_private.p>checkEnvSetup_private at 75
In checkEnvSetup at 156
3. Checking CGT (Code Generation Tools) version
Required version: 6.1.10 to 6.1.18
Required for : Code generation
Your Version : 6.1.12
### Setting environment variable "C6000_CGT_INSTALLDIR" to "C:\Program Files (x86)\Texas Instruments\ccsv4\tools\compiler\c6000"
4. Checking DSP/BIOS (Real Time Operating System) version
Required version: 5.33.05 to 5.41.09.34
Required for : Code generation
Your Version : 5.41.02.14
### Setting environment variable "CCSV4_DSPBIOS_INSTALLDIR" to "C:\Program Files (x86)\Texas Instruments\bios_5_41_02_14"
5. Checking XDC Tools (eXpress DSP Components) version
Required version: 3.16.02.32 or later
Required for : Code generation
Your Version : 3.16.02.32
>>
Hi,
I'm not super familiar with the C6000 workflow, but believe you get the CSL from TI. The error is returning a MATLAB default directory - it has not been set correctly, or it cant locate the correct file. You need to get the CSL, and point MATLAB to the directory it resides in.
-b