This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-CC1310: XDS110 Possibly bricked?

Part Number: LAUNCHXL-CC1310

Tool/software: Code Composer Studio

Hello,

Since this morning i've not been able to connect my LAUNCHXL-CC1310 to my PC via the provided USB cable. When i test the connection via CCS I get this message:

[Start: Texas Instruments XDS110 USB Debug Probe_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\_install\AppData\Local\TEXASI~1\
CCS\ti\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'Feb 13 2017'.
The library build time was '16:06:25'.
The library package version is '6.0.576.0'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.

An error occurred while hard opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-260' (0xfffffefc).
The title is 'SC_ERR_XDS110_OPEN'.

The explanation is:
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the ReadMe.txt file there
for instructions.

[End: Texas Instruments XDS110 USB Debug Probe_0]


So tried to execute the commands xdsdfu -e in the command line, and this is the result:

The README file in there says that i have to connect the JTAG pin TDO to ground, which i tried to do, but did not work. 

Can someone please show me how to solve this problem? for example, show me in a picture which pins they mean exactly by the TDO and GND?

Kind regards,

Jesse