This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC430F6137: MSP430

Part Number: CC430F6137


Tool/software: Code Composer Studio

Hi ,

I followed this thread : 

But no success , the ccs starts downloading MSP430 compiler 4.1 , but crashes midway ?

Is there a link to download offline installation file for MSP430 compiler 4.1  ????

I am using CCS ver5.1.1

Regards,

  • this is error log i get :
    An error occurred while collecting items to be installed
    session context was:(profile=epp.package.cpp, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
    Problems downloading artifact: org.eclipse.update.feature,com.ti.cgt.msp430.4.1.win32,4.1.9.
    Error reading signed content:C:\Users\connekt2\AppData\Local\Temp\signatureFile7484312207342309939.jar
    An error occurred while processing the signatures for the file: C:\Users\connekt2\AppData\Local\Temp\signatureFile7484312207342309939.jar
  • You can get the 4.4.8 compiler here:
    software-dl.ti.com/.../download.htm

    I will see if we can provide a link to 4.1.x.

    I tried installing the 4.1.9 compiler from within my CCSv5.5 and that worked ok. I don't have a 5.1 installation to try. In 5.5 it did ask me to confirm the signature while downloading. It could be that 5.1 doesn't like the digital signature.

    Regards,
    John
  • I found a machine with CCSv5.1.1 and I see the same error that you do when installing the 4.1.9 compiler. I also tried 4.1.8 and 4.1.0 with the same results. CCSv5.1.1 is not able to handle the signature. CCSv5.5 and later are fine.

    Are you able to update to CCSv5.5? If not I can prepare a package.

    John
  • I have the installer uploaded. I will send you a friend request. Once you have accepted that I can send you a private message with the download link for the 4.1.9 installer.

    Regards,
    John
  • I have tried installing CCS ver 5.5 as well with offline installer , it too spite out some error and the installation process was not complete ????

    please do send me the MSP430 compiler 4.1.9 .
  • Ahmed,

    I have sent a private message with the link. When you run the installer if you install under C:\ti then CCS should discover the compiler automatically. If it does not you can point CCSv5.1.1 to it from the Preferences dialog. Window -> Preferences. Then go to Code Composer Studio -> Build -> Compilers in the tree on the left.

    Regards,
    John