Other Parts Discussed in Thread: UCD3138, UCD3138A64
Tool/software: Code Composer Studio
Hi,
I've spent all day trying to install Code Composer and be able to develop for UCD3138. The persisting problem is that not all or none of the necessary files get installed.
I've tried online installers, offline installers, for Linux, for Windows - all not good. The best I've got was half success under Linux: header files were present in ccs_base/arm/include/digital_power/UCD3138, so that I might compile, but not a single file that might define symbols was anywhere, so that linking the code was not possible (a source code file, linker script, assembler nor precompiled binary - I've searched the whole directory tree with grep). Under Windows the header files were missing too.
So, please, let me know where in the tree of Code Composer the files for UCD3138 should be located. Which "package" in the offline installer should contain them? Is it possible to get those files without the whole Code Composer?
I need: header files defining registers, source code/object files defining the corresponding symbols for linking and linker script (preferably for GNU GCC).
Best regards,
Adam