This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/PGA900: Can't get debugging to work with CCSv7 and PGA900 with XDS200 debug probe

Part Number: PGA900

Tool/software: Code Composer Studio

I recently upgraded my toolchain from CCSv6 to CCSv7.  I created a new PGA900 project and used the default configuration.  After a bit of work mucking about with includes I was able to get my old application code to compiler in the new project with the new toolchain, but I can't get the debugger to connect.  The error message I get is:

CS_DAP_0: Error connecting to the target: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.576.0) 

I tried lowering the JTAG speed from the default of 10 MHz to 1 MHz and it had no effect.

If I open PGA900.ccxml and try the "test connection" item, I get the following error message at the end of the output log:

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-230' (0xffffff1a).
The title is 'SC_ERR_PATH_MEASURE'.

The explanation is:
The measured lengths of the JTAG IR and DR scan-paths are invalid.
This indicates that an error exists in the link-delay or scan-path.

[End: Texas Instruments XDS2xx USB Debug Probe]