Part Number: EVMK2H
Other Parts Discussed in Thread: 66AK2H12, 66AK2H14
Tool/software: Code Composer Studio
When using CCS 7.1.0.00016 with Keystone2 device support 1.1.9 for an EVMK2H the list of peripheral register definitions is incomplete.
I haven't generated a complete list of missing peripheral register definitions, but a summary of the types of issue are:
1) There is no device file for a 66AK2H14, so have to use the closest match of 66AK2H12.
2) For the ARM Cortex-A15 cores only the CPU core registers are shown, there are no peripheral registers. i.e. have to connect to a C66xx core to display the peripheral registers.
3) For peripherals with an "array" of registers, e.g. Power Domain Status Register PDSTAT0 to PDSTAT31 registers only the first register is shown, with comments about the number and stride of the registers. E.g.:
Therefore, the memory browser has to be used to inspect registers other than the first in an "array".
4) There are no peripheral registers for the Gigabit Ethernet Switch Subsystem (base address 0x02090000) part of the Network Coprocessor.
Is it possible that the the device XML files could include all the peripheral registers for the 66AK2H14?