Part Number: CC2650STK
Tool/software: Code Composer Studio
Hello,
i have a Problem to build my Project. I've taken the simple ble peripheral example for the CC2650STK and made all files local.
But now I am facing this big issue with the Memory allocation. I get the following error in the linking phase:
------------------------------------------------------------------------------------------------------------------------------------
<Linking>
"configPkg/linker.cmd", line 596: warning #10096-D: specified address lies outside memory map
error #10264: DEFAULT memory range overlaps existing memory range IMAGE_HEADER
error #10264: DEFAULT memory range overlaps existing memory range FLASH
error #10264: DEFAULT memory range overlaps existing memory range SRAM
"configPkg/linker.cmd", line 721: warning #10096-D: specified address lies outside memory map
error #10263: DEFAULT memory range has already been specified
error #10264: DEFAULT memory range overlaps existing memory range DEFAULT
error #10264: DEFAULT memory range overlaps existing memory range IMAGE_HEADER
error #10264: DEFAULT memory range overlaps existing memory range FLASH
error #10264: DEFAULT memory range overlaps existing memory range SRAM
error #10010: errors encountered during linking; "simple_peripheral_cc2650stk_app_local.out" not built
------------------------------------------------------------------------------------------------------------------------------------
I've read some other entries in These Forums, but I couldn't solve this by myself.
in my Project there are several .cmd files, but i don't think they interfere in any way.
/cfs-file/__key/communityserver-discussions-components-files/81/Command_5F00_files.7z
Does anyone have a solution to my Problem.
Thanks in Advance ;)
Kind regards,
Alexander