Tool/software: Code Composer Studio
I installed the latest 7.1 Code Composer as we are migrating from version 6.0.0 after 3 years of good work with the old version. Time to catch up now that things are slow.
I used an existing project which got updated to the newer format for projects. When I built the project there were errors (no surprise there), but the window pane for Problems and also Advice are not displayed. Going to View->Problems and View->Advice do not show either pane as I had in my original project. I deleted CCS V7.1 since it had errors of some sort and was suspect. I opened the failing project back in v6.0.0 and the Problems view still does not show up. I did a Winmerge on the .metadata directory from a working 6.0.0 workspace and my 7.1 modified workspace. There are massive differences in some files and it is not obvious what might be causing the issue.
It looks like workbench.xmi might be the source of the issue.
Any pointers on how to get Eclipse to display the ProblemsView pane? Also ideas why it is happening?
Thanks.