Other Parts Discussed in Thread: CC2640
Tool/software: Code Composer Studio
Hi,
I'm trying to port a CC2640 4x4 custom application from ble_sdk_2_02_01_18
to simplelink_cc2640r2_sdk_1_35_00_33 stack.
I am using CCS7.1.0.
If I try to add a new directory to include options, CCS is unable to create a valid
link. When I link files into the application, I am using TL_BLE_SDK_BASE as
the base link. A screenshot of include options is attached. What is causing this
problem?
Thanks,
Priya