This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv4 output console shared for debug and project perspectives



hi,

 

I noticed that the output console is shared between the debug and the c/C++ project perspectives: The data coming from printf in the running applications can be merged with the output of the build.

since I have a long application runtime , i would like to be able to launch a compilation without having the console windows displaying the test results (further saved as a log result) bothered by the compilation messages.

Is it possible to do so?

 

I am using CCV4.2.m9 on XP, for omap4430 devices

 

regards

  • Claudio,

    If I understood correctly your question, the console view has several overlayed panes and each contains a type of output.

    Check the screen attached; you can click on the small triangle and select which view you would like to display: Build, GEL output or CIO for each core of your device.

    Hope this helps,

    Rafael