This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS UPDATE CAUSED INCREASED CROSS PATH STALLS



I was using CCS3.3  6482 simulator, with cgt 6.0.16, bios 5.31, and SR4( 3.3.50), everything went well.

Days ago I updated CCS to cgt 6.0.25, bios 5.33.06,and SR 11(3.3.81.6), and I compiled the same project ,then run it. Somthing surprising is that

I saw the "Cross Path Stalls " in the profile window came to be 3.6%,  wheras it was just 0.2% in the version before updating.

I did some test  and found that , the SR11 update seems to cause the problem. If I keep SR4(3.3.50), whatever the cgt or bios is, no increasing of cross path stalls could be seen.

About CROSS PATH STALL  concerning C64+ SPLOOP, it is said the cgt 6.0.25 or later could be a fix.

My prject is a codec, contains both C files and assembly files .And the expense calculated by clock() in MCPS increased by 0.3MCPS, which is huge to me .

Is the  increased cross path stalls caused by the compiled C files?Since the assembly files should not be reprocessed by assembler.

So , why do the updated components seem not so effective to my project,  what's the real reason, and  WHAT CAN  I  DO?

Thanks in advance.