Part Number: AM5728
Tool/software: Code Composer Studio
Hello,
I have TI AM572x EVM. Just bought XDS200 JTAG debugger and trying to run a program on the target from the host. I have few questions.
1) When I create a new CCS project, as can be seen in the video attached, I chose the correct target and the debugger. Does it automatically choose the endianness too? Because I am getting "does not match the target endianness not loaded" error. When I change the endianness to little, I get "a data verification error occurred file load failed" error.
2) Why is the linker command file setting empty? Shouldn't all of this automatic? Which linker command file should I choose in this case? I could not find anything specific to AM5728.
3) Once the project is created, there is a red cross on the target configuration file. As can be seen in the video attached. When, I have specified all of this information while creating the CCS project why does it show a red cross on it?
Thank you very much for your time.