This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CCSTUDIO-SITARA: Error Getting PRU .bin file from ccs v7

Part Number: CCSTUDIO-SITARA

Tool/software: Code Composer Studio

Hi,

The CCS v6 works well for generating PRU .bin files. However, when I upgraded to CCSv7 the same project could not generate the PRU .bin files. Do I have to make any extra modifications to the CCSv7 configuration?

Thank you.

  • Hello,

    The error occurs because the hex utility could not find the *.out file to convert. It is looking in C:/Users for the TIAGO.out file. I assume that is the wrong location to look and the wrong name for the *.out file. I can see that your user name has a white space in it. Hence many of your paths have a whitespace in it also. Sometimes a whitespace can cause issues. Were you using the same user name when using CCSv6?

    Thanks

    ki

  • Ki-Soo Lee said:
    Were you using the same user name when using CCSv6?

    Or perhaps when using CCSv6, you had your workspace folder in a location without whitespaces in the path. Try using a new location for your workspace, one without whitespaces.

    Thanks

    ki

  • Hi Ki!
    I did what you suggest and works fine now.
    Thanks a lot!!