Part Number: TM4C129ENCPDT
Tool/software: Code Composer Studio
Under Project Properties -> General, the field for Linker Command File goes blank inexplicably.
We are using CCSv7 version 7.1.0.00016 with both TI and GNU Compilers to code for TM4C series MCUs. The project was originally created for TI compiler. Subsequently we followed the instructions here: processors.wiki.ti.com/.../Using_GCC_with_Tiva_in_CCSv6 to add a build configuration for GNU GCC (Linaro). The compiler versions are: ti-cgt-arm_16.9.3.LTS and gcc-arm-none-eabi-4_9-2015q3.
Our projects are checked into a version control system following the advice here: processors.wiki.ti.com/.../Source_control_with_CCS namely that we checked in .ccsproject, .cproject, .project, the .settings folder, and we did NOT check in the following: \Debug or \Release or other build artifact folders, .config, or .launches folders. We did not check in the targetConfigs folder either because we are using "Manage the project's target configuration automatically" and on examination of the files therein it appears they have nothing to do with the build process. We also followed the advice here: processors.wiki.ti.com/.../Portable_Projects to make the project portable, as multiple users on multiple computers may check the project out of version control and work on it. One other thing we did was to copy the tm4c129encpdt.lds file (this is the GNU linker command file) into the project directory, to maintain consistency, as the tm4c129encpdt.cmd (TI linker command file) is in the project directory. We renamed tm4c129encpdt.lds to tm4c129encpdt_gcc.lds for consistency with the tm4c129encpdt_startup_css_gcc.c file that was created when the GNU build configuration was added. We set this name in Project Properties -> General, in the field for Linker Command File. After testing that building succeeded, we committed the project state to version control.
To test that the project is, in fact, portable, we checked it out to a fresh directory and subsequently imported it into a new CCS workspace. When we examined the settings to make sure that nothing was lost, we noticed that the above mentioned field for Linker Command File (under Project Properties -> General) is now blank. Strangely, the build seems to succeed anyway, and the linker command references this file:
'Invoking: GNU Linker'
"C:/ti/ccsv7/tools/compiler/gcc-arm-none-eabi-4_9-2015q3/bin/arm-none-eabi-gcc.exe" -DPART_TM4C129ENCPDT -DTARGET_IS_TM4C129_RA0 -ffunction-sections -fdata-sections -g -gdwarf-3 -gstrict-dwarf -Wall -MD -std=c99 -march=armv7e-m -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -Wl,-Map,"Master.map" --entry _start -L"C:/ti/TivaWare_C_Series-2.1.4.178/driverlib/gcc" -o"Master.out" "./main.o" "./tm4c129encpdt_startup_ccs_gcc.o" -Wl,-T"../tm4c129encpdt_gcc.lds" -Wl,--start-group -lc -lgcc -lnosys -ldriver -Wl,--end-group
'Finished building target: Master.out'
We are concerned that this may be a bug. Also we are concerned that altering any other setting in Project Properties and applying the changes would apply the now-incorrect contents of this field and lose the linker command file setting.
It is of the utmost importance that project state is preserved when committing and checking out of version control, and that no project settings that affect the build are lost.