Other Parts Discussed in Thread: CC3100, CC3200, MSP432WARE
Tool/software: TI C/C++ Compiler
I'm looking for a TI-RTOS MQTT solution for the CC3100 Booster pack and MSP432 but have not found one thus far. I did import the CC3100BOST_MQTT_TwitterLED_MSP432P401R example and with some modification was able to Publish and Subscribe to topics via a Mosquitto Broker running on a Beaglebone. This example is pretty much what I would like to implement in TI-RTOS with the GNU Compiler and C++ so I attempted to port over the Twitter example and am running into some resolution errors.
One such is
undefined first referenced
symbol in file
--------- ----------------
_SlNonOsMainLoopTask ./tcpEchoCC3X00.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT.out" not built
>> Compilation failure
makefile:163: recipe for target 'tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT.out' failed
gmake: *** [tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT.out] Error 1
gmake: Target 'all' not remade because of errors.
**** Build Finished ****
I've included the paths to includes for the items that are showing errors so I am not sure why the compiler can not location these includes.
I've attached the config file for the project as a reference and included the console output from the compile session which shows the error.
Any assist I can get on this would be most helpful.
CCS version: 6.2
Compiler version: GNU v4.9.3 (Linaro)
codegenToolVersion = "15.12.4.LTS
MSP432 TI-RTOS version: 2_20_00_06
MSP430 Tools version: 3_32_00_06
//////////////tcpECHOCC3x00_MSP **** Build of configuration Debug for project tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT **** "C:\\ti\\ccsv6_2\\ccsv6\\utils\\bin\\gmake" -k all 'Building file: ../tcpEchoCC3X00.cfg' 'Invoking: XDCtools' "C:/ti/xdctools_3_32_00_06_core/xs" --xdcpath="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/packages;C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/bios_6_46_00_23/packages;C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages;C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/uia_2_00_06_52/packages;C:/ti/ccsv6_2/ccsv6/ccs_base;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.M4F -p ti.platforms.msp432:MSP432P401R -r release -c "C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS" --compileOptions "-mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path=\"C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include\" --include_path=\"C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include/CMSIS\" --include_path=\"C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/oslib\" --include_path=\"C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink\" --include_path=\"C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/source\" --include_path=\"C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/include\" --include_path=\"C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/eclipse/plugins/com.ti.mcu.msp432.driverlib.product.ui_3.21.0.05/resources/empty/MSP432P4xx/driverlib/MSP432P4xx\" --include_path=\"C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/board\" --include_path=\"C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/cli_uart\" --include_path=\"C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/mqtt\" --include_path=\"C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT\" --include_path=\"C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc/CMSIS\" --include_path=\"C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc\" --include_path=\"C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/driverlib/MSP432P4xx\" --include_path=\"C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/include\" --advice:power_severity=suppress --advice:power=all -g --gcc --define=__MSP432P401R__ --define=TARGET_IS_MSP432P4XX --define=ccs --define=SL_FULL --define=MSP432WARE --define=_USE_CLI_ --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi " "../tcpEchoCC3X00.cfg" making package.mak (because of package.bld) ... generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ... configuring tcpEchoCC3X00.xem4f from package/cfg/tcpEchoCC3X00_pem4f.cfg ... generating custom ti.sysbios library makefile ... Starting build of library sources ... making C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/src/sysbios/sysbios.aem4f ... gmake[1]: Entering directory `C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/src/sysbios' clem4f C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/bios_6_46_00_23/packages/ti/sysbios/BIOS.c ... asmem4f C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/bios_6_46_00_23/packages/ti/sysbios/family/arm/m3/Hwi_asm.sv7M ... asmem4f C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/bios_6_46_00_23/packages/ti/sysbios/family/arm/m3/Hwi_asm_switch.sv7M ... asmem4f C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/bios_6_46_00_23/packages/ti/sysbios/family/arm/m3/IntrinsicsSupport_asm.sv7M ... asmem4f C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/bios_6_46_00_23/packages/ti/sysbios/family/arm/m3/TaskSupport_asm.sv7M ... arem4f BIOS.obj m3_Hwi_asm.obj m3_Hwi_asm_switch.obj m3_IntrinsicsSupport_asm.obj m3_TaskSupport_asm.obj ... gmake[1]: Leaving directory `C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/src/sysbios' Build of libraries done. clem4f package/cfg/tcpEchoCC3X00_pem4f.c ... 'Finished building: ../tcpEchoCC3X00.cfg' ' ' 1 file(s) copied. making ../src/sysbios/sysbios.aem4f ... gmake[1]: Entering directory 'C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/src/sysbios' gmake[1]: Nothing to be done for 'all'. gmake[1]: Leaving directory 'C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/src/sysbios' 'Building file: ../MSP_EXP432P401R.c' 'Invoking: MSP432 Compiler' "C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include" --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/oslib" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/source" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/include" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/eclipse/plugins/com.ti.mcu.msp432.driverlib.product.ui_3.21.0.05/resources/empty/MSP432P4xx/driverlib/MSP432P4xx" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/board" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/cli_uart" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/mqtt" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/driverlib/MSP432P4xx" --include_path="C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/include" --advice:power_severity=suppress --advice:power=all -g --gcc --define=__MSP432P401R__ --define=TARGET_IS_MSP432P4XX --define=ccs --define=SL_FULL --define=MSP432WARE --define=_USE_CLI_ --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="MSP_EXP432P401R.d" --cmd_file="configPkg/compiler.opt" "../MSP_EXP432P401R.c" 'Finished building: ../MSP_EXP432P401R.c' ' ' 'Building file: ../sockets.c' 'Invoking: MSP432 Compiler' "C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include" --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/oslib" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/source" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/include" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/eclipse/plugins/com.ti.mcu.msp432.driverlib.product.ui_3.21.0.05/resources/empty/MSP432P4xx/driverlib/MSP432P4xx" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/board" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/cli_uart" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/mqtt" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/driverlib/MSP432P4xx" --include_path="C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/include" --advice:power_severity=suppress --advice:power=all -g --gcc --define=__MSP432P401R__ --define=TARGET_IS_MSP432P4XX --define=ccs --define=SL_FULL --define=MSP432WARE --define=_USE_CLI_ --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="sockets.d" --cmd_file="configPkg/compiler.opt" "../sockets.c" 'Finished building: ../sockets.c' ' ' 'Building file: ../tcpEchoCC3X00.c' 'Invoking: MSP432 Compiler' "C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include" --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/oslib" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/source" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/include" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/eclipse/plugins/com.ti.mcu.msp432.driverlib.product.ui_3.21.0.05/resources/empty/MSP432P4xx/driverlib/MSP432P4xx" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/board" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/cli_uart" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/mqtt" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/driverlib/MSP432P4xx" --include_path="C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/include" --advice:power_severity=suppress --advice:power=all -g --gcc --define=__MSP432P401R__ --define=TARGET_IS_MSP432P4XX --define=ccs --define=SL_FULL --define=MSP432WARE --define=_USE_CLI_ --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="tcpEchoCC3X00.d" --cmd_file="configPkg/compiler.opt" "../tcpEchoCC3X00.c" "../tcpEchoCC3X00.c", line 164: warning #69-D: integer conversion resulted in a change of sign "../tcpEchoCC3X00.c", line 347: warning #179-D: variable "rc" was declared but never referenced "../tcpEchoCC3X00.c", line 395: warning #225-D: function "initClk" declared implicitly "../tcpEchoCC3X00.c", line 606: warning #225-D: function "Delay" declared implicitly "../tcpEchoCC3X00.c", line 608: warning #112-D: statement is unreachable "../tcpEchoCC3X00.c", line 679: warning #225-D: function "strtol" declared implicitly "../tcpEchoCC3X00.c", line 711: warning #169-D: argument of type "int" is incompatible with parameter of type "unsigned char *" "../tcpEchoCC3X00.c", line 714: warning #225-D: function "MAP_Timer_A_startCounter" declared implicitly "../tcpEchoCC3X00.c", line 724: warning #169-D: argument of type "char *" is incompatible with parameter of type "unsigned char *" "../tcpEchoCC3X00.c", line 727: warning #225-D: function "MAP_Timer_A_startCounter" declared implicitly "../tcpEchoCC3X00.c", line 748: warning #225-D: function "MAP_Timer_A_clearCaptureCompareInterrupt" declared implicitly "../tcpEchoCC3X00.c", line 791: warning #225-D: function "_SlNonOsMainLoopTask" declared implicitly "../tcpEchoCC3X00.c", line 835: warning #225-D: function "_SlNonOsMainLoopTask" declared implicitly "../tcpEchoCC3X00.c", line 904: warning #225-D: function "_SlNonOsMainLoopTask" declared implicitly 'Finished building: ../tcpEchoCC3X00.c' ' ' 'Building file: ../board/board.c' 'Invoking: MSP432 Compiler' "C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include" --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/oslib" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/source" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/include" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/eclipse/plugins/com.ti.mcu.msp432.driverlib.product.ui_3.21.0.05/resources/empty/MSP432P4xx/driverlib/MSP432P4xx" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/board" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/cli_uart" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/mqtt" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/driverlib/MSP432P4xx" --include_path="C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/include" --advice:power_severity=suppress --advice:power=all -g --gcc --define=__MSP432P401R__ --define=TARGET_IS_MSP432P4XX --define=ccs --define=SL_FULL --define=MSP432WARE --define=_USE_CLI_ --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="board/board.d" --obj_directory="board" --cmd_file="configPkg/compiler.opt" "../board/board.c" 'Finished building: ../board/board.c' ' ' 'Building file: ../cli_uart/cli_uart.c' 'Invoking: MSP432 Compiler' "C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include" --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/oslib" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/source" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/include" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/eclipse/plugins/com.ti.mcu.msp432.driverlib.product.ui_3.21.0.05/resources/empty/MSP432P4xx/driverlib/MSP432P4xx" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/board" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/cli_uart" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/mqtt" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/driverlib/MSP432P4xx" --include_path="C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/include" --advice:power_severity=suppress --advice:power=all -g --gcc --define=__MSP432P401R__ --define=TARGET_IS_MSP432P4XX --define=ccs --define=SL_FULL --define=MSP432WARE --define=_USE_CLI_ --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="cli_uart/cli_uart.d" --obj_directory="cli_uart" --cmd_file="configPkg/compiler.opt" "../cli_uart/cli_uart.c" "../cli_uart/cli_uart.c", line 113: warning #225-D: function "PCM_gotoLPM0" declared implicitly 'Finished building: ../cli_uart/cli_uart.c' ' ' 'Building file: ../mqtt/MQTTCC3100.c' 'Invoking: MSP432 Compiler' "C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include" --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/oslib" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/source" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/include" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/eclipse/plugins/com.ti.mcu.msp432.driverlib.product.ui_3.21.0.05/resources/empty/MSP432P4xx/driverlib/MSP432P4xx" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/board" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/cli_uart" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/mqtt" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/driverlib/MSP432P4xx" --include_path="C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/include" --advice:power_severity=suppress --advice:power=all -g --gcc --define=__MSP432P401R__ --define=TARGET_IS_MSP432P4XX --define=ccs --define=SL_FULL --define=MSP432WARE --define=_USE_CLI_ --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="mqtt/MQTTCC3100.d" --obj_directory="mqtt" --cmd_file="configPkg/compiler.opt" "../mqtt/MQTTCC3100.c" "../mqtt/MQTTCC3100.c", line 111: warning #169-D: argument of type "char *" is incompatible with parameter of type "_i8 *" "../mqtt/MQTTCC3100.c", line 172: warning #169-D: argument of type "char *" is incompatible with parameter of type "_i8 *" 'Finished building: ../mqtt/MQTTCC3100.c' ' ' 'Building file: ../mqtt/MQTTClient.c' 'Invoking: MSP432 Compiler' "C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include" --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/oslib" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/source" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/include" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/eclipse/plugins/com.ti.mcu.msp432.driverlib.product.ui_3.21.0.05/resources/empty/MSP432P4xx/driverlib/MSP432P4xx" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/board" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/cli_uart" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/mqtt" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/driverlib/MSP432P4xx" --include_path="C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/include" --advice:power_severity=suppress --advice:power=all -g --gcc --define=__MSP432P401R__ --define=TARGET_IS_MSP432P4XX --define=ccs --define=SL_FULL --define=MSP432WARE --define=_USE_CLI_ --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="mqtt/MQTTClient.d" --obj_directory="mqtt" --cmd_file="configPkg/compiler.opt" "../mqtt/MQTTClient.c" 'Finished building: ../mqtt/MQTTClient.c' ' ' 'Building file: ../mqtt/MQTTConnectClient.c' 'Invoking: MSP432 Compiler' "C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include" --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/oslib" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/source" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/include" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/eclipse/plugins/com.ti.mcu.msp432.driverlib.product.ui_3.21.0.05/resources/empty/MSP432P4xx/driverlib/MSP432P4xx" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/board" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/cli_uart" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/mqtt" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/driverlib/MSP432P4xx" --include_path="C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/include" --advice:power_severity=suppress --advice:power=all -g --gcc --define=__MSP432P401R__ --define=TARGET_IS_MSP432P4XX --define=ccs --define=SL_FULL --define=MSP432WARE --define=_USE_CLI_ --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="mqtt/MQTTConnectClient.d" --obj_directory="mqtt" --cmd_file="configPkg/compiler.opt" "../mqtt/MQTTConnectClient.c" 'Finished building: ../mqtt/MQTTConnectClient.c' ' ' 'Building file: ../mqtt/MQTTConnectServer.c' 'Invoking: MSP432 Compiler' "C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include" --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/oslib" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/source" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/include" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/eclipse/plugins/com.ti.mcu.msp432.driverlib.product.ui_3.21.0.05/resources/empty/MSP432P4xx/driverlib/MSP432P4xx" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/board" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/cli_uart" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/mqtt" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/driverlib/MSP432P4xx" --include_path="C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/include" --advice:power_severity=suppress --advice:power=all -g --gcc --define=__MSP432P401R__ --define=TARGET_IS_MSP432P4XX --define=ccs --define=SL_FULL --define=MSP432WARE --define=_USE_CLI_ --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="mqtt/MQTTConnectServer.d" --obj_directory="mqtt" --cmd_file="configPkg/compiler.opt" "../mqtt/MQTTConnectServer.c" 'Finished building: ../mqtt/MQTTConnectServer.c' ' ' 'Building file: ../mqtt/MQTTDeserializePublish.c' 'Invoking: MSP432 Compiler' "C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include" --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/oslib" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/source" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/include" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/eclipse/plugins/com.ti.mcu.msp432.driverlib.product.ui_3.21.0.05/resources/empty/MSP432P4xx/driverlib/MSP432P4xx" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/board" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/cli_uart" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/mqtt" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/driverlib/MSP432P4xx" --include_path="C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/include" --advice:power_severity=suppress --advice:power=all -g --gcc --define=__MSP432P401R__ --define=TARGET_IS_MSP432P4XX --define=ccs --define=SL_FULL --define=MSP432WARE --define=_USE_CLI_ --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="mqtt/MQTTDeserializePublish.d" --obj_directory="mqtt" --cmd_file="configPkg/compiler.opt" "../mqtt/MQTTDeserializePublish.c" 'Finished building: ../mqtt/MQTTDeserializePublish.c' ' ' 'Building file: ../mqtt/MQTTFormat.c' 'Invoking: MSP432 Compiler' "C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include" --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/oslib" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/source" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/include" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/eclipse/plugins/com.ti.mcu.msp432.driverlib.product.ui_3.21.0.05/resources/empty/MSP432P4xx/driverlib/MSP432P4xx" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/board" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/cli_uart" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/mqtt" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/driverlib/MSP432P4xx" --include_path="C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/include" --advice:power_severity=suppress --advice:power=all -g --gcc --define=__MSP432P401R__ --define=TARGET_IS_MSP432P4XX --define=ccs --define=SL_FULL --define=MSP432WARE --define=_USE_CLI_ --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="mqtt/MQTTFormat.d" --obj_directory="mqtt" --cmd_file="configPkg/compiler.opt" "../mqtt/MQTTFormat.c" "../mqtt/MQTTFormat.c", line 122: warning #552-D: variable "strindex" was set but never used "../mqtt/MQTTFormat.c", line 200: warning #552-D: variable "rc" was set but never used "../mqtt/MQTTFormat.c", line 190: warning #552-D: variable "strindex" was set but never used 'Finished building: ../mqtt/MQTTFormat.c' ' ' 'Building file: ../mqtt/MQTTPacket.c' 'Invoking: MSP432 Compiler' "C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include" --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/oslib" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/source" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/include" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/eclipse/plugins/com.ti.mcu.msp432.driverlib.product.ui_3.21.0.05/resources/empty/MSP432P4xx/driverlib/MSP432P4xx" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/board" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/cli_uart" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/mqtt" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/driverlib/MSP432P4xx" --include_path="C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/include" --advice:power_severity=suppress --advice:power=all -g --gcc --define=__MSP432P401R__ --define=TARGET_IS_MSP432P4XX --define=ccs --define=SL_FULL --define=MSP432WARE --define=_USE_CLI_ --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="mqtt/MQTTPacket.d" --obj_directory="mqtt" --cmd_file="configPkg/compiler.opt" "../mqtt/MQTTPacket.c" 'Finished building: ../mqtt/MQTTPacket.c' ' ' 'Building file: ../mqtt/MQTTSerializePublish.c' 'Invoking: MSP432 Compiler' "C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include" --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/oslib" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/source" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/include" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/eclipse/plugins/com.ti.mcu.msp432.driverlib.product.ui_3.21.0.05/resources/empty/MSP432P4xx/driverlib/MSP432P4xx" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/board" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/cli_uart" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/mqtt" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/driverlib/MSP432P4xx" --include_path="C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/include" --advice:power_severity=suppress --advice:power=all -g --gcc --define=__MSP432P401R__ --define=TARGET_IS_MSP432P4XX --define=ccs --define=SL_FULL --define=MSP432WARE --define=_USE_CLI_ --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="mqtt/MQTTSerializePublish.d" --obj_directory="mqtt" --cmd_file="configPkg/compiler.opt" "../mqtt/MQTTSerializePublish.c" 'Finished building: ../mqtt/MQTTSerializePublish.c' ' ' 'Building file: ../mqtt/MQTTSubscribeClient.c' 'Invoking: MSP432 Compiler' "C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include" --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/oslib" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/source" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/include" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/eclipse/plugins/com.ti.mcu.msp432.driverlib.product.ui_3.21.0.05/resources/empty/MSP432P4xx/driverlib/MSP432P4xx" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/board" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/cli_uart" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/mqtt" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/driverlib/MSP432P4xx" --include_path="C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/include" --advice:power_severity=suppress --advice:power=all -g --gcc --define=__MSP432P401R__ --define=TARGET_IS_MSP432P4XX --define=ccs --define=SL_FULL --define=MSP432WARE --define=_USE_CLI_ --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="mqtt/MQTTSubscribeClient.d" --obj_directory="mqtt" --cmd_file="configPkg/compiler.opt" "../mqtt/MQTTSubscribeClient.c" 'Finished building: ../mqtt/MQTTSubscribeClient.c' ' ' 'Building file: ../mqtt/MQTTSubscribeServer.c' 'Invoking: MSP432 Compiler' "C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include" --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/oslib" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/source" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/include" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/eclipse/plugins/com.ti.mcu.msp432.driverlib.product.ui_3.21.0.05/resources/empty/MSP432P4xx/driverlib/MSP432P4xx" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/board" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/cli_uart" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/mqtt" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/driverlib/MSP432P4xx" --include_path="C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/include" --advice:power_severity=suppress --advice:power=all -g --gcc --define=__MSP432P401R__ --define=TARGET_IS_MSP432P4XX --define=ccs --define=SL_FULL --define=MSP432WARE --define=_USE_CLI_ --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="mqtt/MQTTSubscribeServer.d" --obj_directory="mqtt" --cmd_file="configPkg/compiler.opt" "../mqtt/MQTTSubscribeServer.c" 'Finished building: ../mqtt/MQTTSubscribeServer.c' ' ' 'Building file: ../mqtt/MQTTUnsubscribeClient.c' 'Invoking: MSP432 Compiler' "C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include" --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/oslib" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/source" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/include" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/eclipse/plugins/com.ti.mcu.msp432.driverlib.product.ui_3.21.0.05/resources/empty/MSP432P4xx/driverlib/MSP432P4xx" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/board" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/cli_uart" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/mqtt" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/driverlib/MSP432P4xx" --include_path="C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/include" --advice:power_severity=suppress --advice:power=all -g --gcc --define=__MSP432P401R__ --define=TARGET_IS_MSP432P4XX --define=ccs --define=SL_FULL --define=MSP432WARE --define=_USE_CLI_ --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="mqtt/MQTTUnsubscribeClient.d" --obj_directory="mqtt" --cmd_file="configPkg/compiler.opt" "../mqtt/MQTTUnsubscribeClient.c" 'Finished building: ../mqtt/MQTTUnsubscribeClient.c' ' ' 'Building file: ../mqtt/MQTTUnsubscribeServer.c' 'Invoking: MSP432 Compiler' "C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include" --include_path="C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/oslib" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/source" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/tidrivers_msp43x_2_20_00_08/packages/ti/mw/wifi/cc3x00/simplelink/include" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/eclipse/plugins/com.ti.mcu.msp432.driverlib.product.ui_3.21.0.05/resources/empty/MSP432P4xx/driverlib/MSP432P4xx" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/board" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/cli_uart" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT/mqtt" --include_path="C:/Users/jomodev/workspace_v6_2/tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc/CMSIS" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/inc" --include_path="C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/driverlib/MSP432P4xx" --include_path="C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/include" --advice:power_severity=suppress --advice:power=all -g --gcc --define=__MSP432P401R__ --define=TARGET_IS_MSP432P4XX --define=ccs --define=SL_FULL --define=MSP432WARE --define=_USE_CLI_ --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --preproc_with_compile --preproc_dependency="mqtt/MQTTUnsubscribeServer.d" --obj_directory="mqtt" --cmd_file="configPkg/compiler.opt" "../mqtt/MQTTUnsubscribeServer.c" 'Finished building: ../mqtt/MQTTUnsubscribeServer.c' ' ' 'Building target: tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT.out' 'Invoking: MSP432 Linker' "C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --advice:power_severity=suppress --advice:power=all -g --gcc --define=__MSP432P401R__ --define=TARGET_IS_MSP432P4XX --define=ccs --define=SL_FULL --define=MSP432WARE --define=_USE_CLI_ --diag_warning=225 --diag_warning=255 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi -z -m"tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT.map" --stack_size=512 --heap_size=1024 -i"C:/ti/ccsv6_2/ccsv6/ccs_base/arm/include" -i"C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/lib" -i"C:/ti/ccsv6_2/ccsv6/tools/compiler/ti-cgt-arm_15.12.4.LTS/include" --reread_libs --warn_sections --diag_wrap=off --display_error_number --xml_link_info="tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT_linkInfo.xml" --rom_model -o "tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT.out" "./MSP_EXP432P401R.obj" "./sockets.obj" "./tcpEchoCC3X00.obj" "./board/board.obj" "./cli_uart/cli_uart.obj" "./mqtt/MQTTCC3100.obj" "./mqtt/MQTTClient.obj" "./mqtt/MQTTConnectClient.obj" "./mqtt/MQTTConnectServer.obj" "./mqtt/MQTTDeserializePublish.obj" "./mqtt/MQTTFormat.obj" "./mqtt/MQTTPacket.obj" "./mqtt/MQTTSerializePublish.obj" "./mqtt/MQTTSubscribeClient.obj" "./mqtt/MQTTSubscribeServer.obj" "./mqtt/MQTTUnsubscribeClient.obj" "./mqtt/MQTTUnsubscribeServer.obj" "../MSP_EXP432P401R.cmd" -l"configPkg/linker.cmd" -l"C:/ti/tirex-content/tirtos_msp43x_2_20_00_06/products/msp432_driverlib_3_21_00_05/driverlib/MSP432P4xx/ccs/msp432p4xx_driverlib.lib" -llibc.a <Linking> warning #10247-D: creating output section ".vtable" without a SECTIONS specification undefined first referenced symbol in file --------- ---------------- _SlNonOsMainLoopTask ./tcpEchoCC3X00.obj error #10234-D: unresolved symbols remain error #10010: errors encountered during linking; "tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT.out" not built >> Compilation failure makefile:163: recipe for target 'tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT.out' failed gmake: *** [tcpEchoCC3X00_MSP_EXP432P401R_TI_MQTT.out] Error 1 gmake: Target 'all' not remade because of errors. **** Build Finished ****