This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
Hi :)
i have trouble using Uniflash under Ubuntu 16.04 (in VirtualBox).
Its not possible to flash anything using CCS directly or Uniflash 4.3 or the newest Uniflash version.
I also tried with loadti and got the following error
***** DSS Generic Loader *****
START: 13:08:47 GMT+0200 (CEST)
Configuring Debug Server for specified target...
Done
TARGET: Texas Instruments XDS100v2 USB Debug Probe
Connecting to target...
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0
testEnv.outFiles: .../Debug/test.out
Loading .../Debug/test.out
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
SEVERE: CortexR4: File Loader: Memory write failed: Timed out waiting for target to halt while executing wr_pll.alg
SEVERE: CortexR4: GEL: File: .../Debug/test.out: Load failed.
SEVERE: File: .../Debug/test.out: Load failed.
SEVERE: Error loading ".../Debug/test.out": File: .../Debug/test.out: Load failed.
Error code #4011, .../Debug/test.out load failed!
Aborting!
Does anyone have an idea??
Best regards,
Malte