Part Number: MSP432P401R
Other Parts Discussed in Thread: ENERGIA
Tool/software: Code Composer Studio
Hello,
I want include ccs code in Energia sketch of ccs... I will try to explain what i want to do...
My code is simple. My code in Energia is the example AnalogReadSerial.
And now i want to add the following code:
_______________________________________________________________________
#include <xdc/std.h>
#include <xdc/runtime/System.h>
/* TI-RTOS Header files */
#include <ti/drivers/GPIO.h>
#include <ti/drivers/PWM.h>
/* Example/Board Header files */
#include "Board.h"
int main(void)
{
Board_initGeneral();
Board_initGPIO();
Board_initPWM();
PWM_Handle pwm1;
PWM_Params params;
uint16_t pwmPeriod = 380; // Period and duty in counts
uint16_t duty = pwmPeriod/2;
PWM_Params_init(¶ms);
params.dutyUnits = PWM_DUTY_COUNTS;
params.dutyValue = duty;
params.periodUnits = PWM_PERIOD_COUNTS;
params.periodValue = pwmPeriod;
pwm1 = PWM_open(Board_PWM0, ¶ms);
if (pwm1 == NULL) {
System_abort("Board_PWM0 did not open");
}
PWM_start(pwm1);
}
___________________________________________________________________________
The ccs code is a PWM signal.
I am following a tutorial for the tivacode to Energia but not works with the msp432...
I have tried copying the ccs code in the one of Energia and changing the name of the main one by main_signal but it gives problems to the time to build by the libraries ....
I have tried in all possible ways to add code composer studio libraries to Energia and vice versa but there is no way it works
Thanks.