This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2640R2F: launchxl-cc2640r2

Part Number: CC2640R2F
Other Parts Discussed in Thread: LAUNCHXL-CC2640R2,

Tool/software: Code Composer Studio

HELP REQUEST PLEASE

XDS110 failed on launchxl-cc2640R2

OS win10, Hardware PC:ASUS X751LD-TY300H

When trying to download an exemple:

{

Error connecting to the target:
(Error -260 @ 0x0)
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the ReadMe.txt file there
for instructions.
(Emulation package 6.0.576.0)

}

When trying "Test Connection" on Target configuration :

{

[Start: Texas Instruments XDS110 USB Debug Probe]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\Kodia\AppData\Local\TEXASI~1\CCS\
    ti\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'Feb 13 2017'.
The library build time was '16:06:25'.
The library package version is '6.0.576.0'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.

An error occurred while hard opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-260' (0xfffffefc).
The title is 'SC_ERR_XDS110_OPEN'.

The explanation is:
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the ReadMe.txt file there
for instructions.

[End: Texas Instruments XDS110 USB Debug Probe]

}

I NEED HELP

  • Hi,

    A thorough explanation for this error with suggestions to debug this is shown at section 5.1 of the following page:
    processors.wiki.ti.com/.../Debugging_JTAG_Connectivity_Problems

    Hope this helps,
    Rafael
  • I tried it on Linux , and its ok now .
    So I stop using it on Win 10.

    But I have seen a difference : On linux the XDCTOOL and others ares installed and i have been prompted for that recommandation .
    After that a new firmware have been download on the kit .

    Now it's working on Linux Debian jessie.
    But it still not working on windows.

    thank for your answer I will read your suggestion

    Best regard

    French Guy
  • Hi,

    Thanks for sending the additional details - the board is fine, as well as the USB cable. 

    kodia raoul said:
    But I have seen a difference : On linux the XDCTOOL and others ares installed and i have been prompted for that recommandation .

    If this sentence means you don't see the directories "ccsv7", "xdctools_3_32_02_25_core" and "xdctools_3_50_02_20_core" on the place where you installed CCS, then I suspect that somehow the Windows 10 install was not successful, which could explain the problems with device drivers. 

    Regards,

    Rafael

  • Hi        ----- I NEED URGEND HELP  -----

    i also have Problems with XDC110 as descibed above - i have 2 brand new launchxl-cc2640r2 Launchpads here wich exactly behave the same

    When i Start the Test Connection in the CC2640R2F.ccxml "Test Connection" it prints out:


    [Start: Texas Instruments XDS110 USB Debug Probe]

    Execute the command:

    %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

    [Result]


    -----[Print the board config pathname(s)]------------------------------------

    C:\Users\CASE18\AppData\Local\TEXASI~1\CCS\
        ti\1\0\BrdDat\testBoard.dat

    -----[Print the reset-command software log-file]-----------------------------

    This utility has selected a 100- or 510-class product.
    This utility will load the adapter 'jioxds110.dll'.
    The library build date was 'May  2 2017'.
    The library build time was '12:59:57'.
    The library package version is '6.0.628.1'.
    The library component version is '35.35.0.0'.
    The controller does not use a programmable FPGA.
    The controller has a version number of '5' (0x00000005).
    The controller has an insertion length of '0' (0x00000000).
    This utility will attempt to reset the controller.
    This utility has successfully reset the controller.

    -----[Print the reset-command hardware log-file]-----------------------------

    The scan-path will be reset by toggling the JTAG TRST signal.
    The controller is the XDS110 with USB interface.
    The link from controller to target is direct (without cable).
    The software is configured for XDS110 features.
    The controller cannot monitor the value on the EMU[0] pin.
    The controller cannot monitor the value on the EMU[1] pin.
    The controller cannot control the timing on output pins.
    The controller cannot control the timing on input pins.
    The scan-path link-delay has been set to exactly '0' (0x0000).

    An error occurred while hard opening the controller.

    -----[An error has occurred and this utility has aborted]--------------------

    This error is generated by TI's USCIF driver or utilities.

    The value is '-261' (0xfffffefb).
    The title is 'SC_ERR_XDS110_FAIL'.

    The explanation is:
    Invalid response was received from the XDS110.

    [End: Texas Instruments XDS110 USB Debug Probe]

    I've still updated the XDS Tools Software Drivers. I am using WINDOWS 10 - and don't have LINUX

    the XDC Tools are located as installed : C:\ti\xdctools_3_32_01_22_core

    Any ideas ?

    Thanks Thomas

  • UPS --- Sorry - I've solved the Problem - I was Debugging the uartecho_CC2640R2_LAUNCHXL_tirtos_gcc (GNU) Project instead of the CCS PRoject : uartecho_CC2640R2_LAUNCHXL_tirtos_ccs !!! It works now -
  • but still prompts - Cortex_M3_0: Failed Board Reset: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 6.0.628.1) - but the Code may be debugged