Other Parts Discussed in Thread: TMS320VC5506
Upon installing the new CCS4 update today, I can no longer access my target. This was working before the update, which is the only thing that was changed. Error message is as follows:
Error connecting to the target: Error 0x80000240/-603 Fatal error during: Initialization, OCS,
Reboot did not help.
I tried to roll back the drivers (I'm running XP), but this option was not available.
The update log in \Program Files\Blackhawk indicates that "A driver update is not needed" so I assume that today's update only affected CCS4 on my system, and that the Blackhawk driver files were not altered.
BHReset and BHProbe both pass the tests.
My hardware is described as:
VID:0B1E
PID:8006
S/N: FX2-0001
Board Type: Emulator 2
Hardware Revision: CPU Rev.C
The following test scripts all pass:
DBGJTAG -X adapter,driver=bhjtag3.dll -T control
DBGJTAG -X adapter,driver=bhjtag3.dll -T memory
Moving from the hardware to CCS4, I first tried re-selecting my Target Configuration, but there was no change. I tried deleting my launch configuration under Non-Project Debug Session, and also deleted the targetdb.cache in ...\ccsv4\DebugServer\bin\win32
How do I determine a fix for this error? Should I downgrade to CCS4.1.2? How would I even do that?