Part Number: RM48L952
Tool/software: TI C/C++ Compiler
Hi,
Need some help determining the cause of a TI linker hang, with 100% CPU core usage in a very large RM48L952 project. It is only this project that causes problems, and we have the same problems on both Win10 x32 and Win10 x64 in both debug and release mode, using both CCSV7 GUI and command line eclipsec.
We are not using any optimization and there is no obvious / strange warnings or errors during the compile stage.
I've tried to switch verbose on for the linker, but there is nothing really output at this stage.
Could anyone suggest some things to try?
Thanks
Stomp!