Tool/software: Code Composer Studio
Hi
So I need to use to mmwave sdk. But although I have given the correct path, it always fails to open the required header files. Error #1965
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi
So I need to use to mmwave sdk. But although I have given the correct path, it always fails to open the required header files. Error #1965
**** Build of configuration Debug for project CollDet_2 **** "C:\\ti\\ccsv7\\utils\\bin\\gmake" -k -j 4 all -O 'Building file: ../main.c' 'Invoking: ARM Compiler' "C:/ti/ccsv7/tools/compiler/ti-cgt-arm_16.9.3.LTS/bin/armcl" -mv7R4 --code_state=32 --float_support=VFPv3D16 --include_path="C:/Users/shantan1/workspace_v7/CollDet_2" --include_path="C:/ti/mmwave_sdk_01_00_00_05/packages/ti/alg/mmwavelib" --include_path="C:/ti/ccsv7/tools/compiler/ti-cgt-arm_16.9.3.LTS/include" -g --diag_warning=225 --diag_wrap=off --display_error_number --enum_type=packed --abi=eabi --preproc_with_compile --preproc_dependency="main.d" "../main.c" >> Compilation failure subdir_rules.mk:9: recipe for target 'main.obj' failed "C:/ti/mmwave_sdk_01_00_00_05/packages/ti/alg/mmwavelib/mmwavelib.h", line 85: fatal error #1965: cannot open source file "ti/alg/mmwavelib/src/vecutils/mmwavelib_vecutils.h" 1 catastrophic error detected in the compilation of "../main.c". Compilation terminated. gmake: *** [main.obj] Error 1 gmake: Target 'all' not remade because of errors. **** Build Finished ****
I have attached the build log. Please have a look.
Thanks,
Shantanu