Part Number: CCSTUDIO
Tool/software: Code Composer Studio
Hello,
I have problem with running CCSv6 on Ubuntu. It seems that was happen after OS update 20.06.2017.
There is log from terminal:
eugene@PC:~/ti/ccsv6/eclipse$ ./ccstudio
Segmentation fault (core dumped)
with gdb:
(gdb) run
Starting program: /home/eugene/ti/ccsv6/eclipse/ccstudio
[Thread debugging using libthread_db enabled]
Using host libthread_db library "/lib/i386-linux-gnu/libthread_db.so.1".
process 8605 is executing new program: /home/eugene/ti/ccsv6/eclipse/ccstudio
[Thread debugging using libthread_db enabled]
Using host libthread_db library "/lib/i386-linux-gnu/libthread_db.so.1".
Program received signal SIGSEGV, Segmentation fault.
0xb60ea15b in _expand_stack_to(unsigned char*) () from /home/eugene/ti/ccsv6/eclipse/jre/bin/../lib/i386/client/libjvm.so
(gdb) bt
#0 0xb60ea15b in _expand_stack_to(unsigned char*) () from /home/eugene/ti/ccsv6/eclipse/jre/bin/../lib/i386/client/libjvm.so
#1 0xb60ea1f9 in os::Linux::manually_expand_stack(JavaThread*, unsigned char*) () from /home/eugene/ti/ccsv6/eclipse/jre/bin/../lib/i386/client/libjvm.so
#2 0xb60ee2f3 in os::create_attached_thread(JavaThread*) () from /home/eugene/ti/ccsv6/eclipse/jre/bin/../lib/i386/client/libjvm.so
#3 0xb61bc86b in Threads::create_vm(JavaVMInitArgs*, bool*) () from /home/eugene/ti/ccsv6/eclipse/jre/bin/../lib/i386/client/libjvm.so
#4 0xb5fccb3c in JNI_CreateJavaVM () from /home/eugene/ti/ccsv6/eclipse/jre/bin/../lib/i386/client/libjvm.so
#5 0xb7fd222a in startJavaJNI (libPath=0x805b980 "/home/eugene/ti/ccsv6/eclipse/jre/bin/../lib/i386/client/libjvm.so", vmArgs=0x80eb7c0, progArgs=0x80ea2c8,
jarFile=0x805e470 "/home/eugene/ti/ccsv6/eclipse//plugins/org.eclipse.equinox.launcher_1.3.0.v20140415-2008.jar") at ../eclipseJNI.c:358
#6 0xb7fd3898 in startJavaVM (libPath=0x805b980 "/home/eugene/ti/ccsv6/eclipse/jre/bin/../lib/i386/client/libjvm.so", vmArgs=0x80eb7c0, progArgs=0x80ea2c8,
jarFile=0x805e470 "/home/eugene/ti/ccsv6/eclipse//plugins/org.eclipse.equinox.launcher_1.3.0.v20140415-2008.jar") at ../eclipseNix.c:174
#7 0xb7fcd1f6 in _run (argc=3, argv=0x804f8d0, vmArgs=0x80673c8) at ../eclipse.c:629
#8 0xb7fccc03 in run (argc=3, argv=0x804f8d0, vmArgs=0x8050280) at ../eclipse.c:465
#9 0x080497a9 in main (argc=14, argv=0x804f8d0) at ../eclipseMain.c:332