This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430FR5857: MISRA C and CCS

Part Number: MSP430FR5857


Tool/software: Code Composer Studio

I am writing a code and want to check if it is MISRA C compliant. I switched on the MISRA C option in Project > Properties > General >Advanced Options > MISRA C. But it has only been added with MISRA C 2004. Is there a way to add an add-in or anything of that kind so as to make it compatible with MISRA C 2012? 

And can anyone provide me a method or flowchart of how to go ahead with MISRA C and its documentation so that I write the code in such a way it is compliant and also how to create a compliance matrix? 

Any help would be helpful.  

Thank you in advance.