Other Parts Discussed in Thread: TEST2
I'm duplicating this question received originally on the TMS570 ARM® Cortex-R4F Transportation and Safety MCUsForum.
Regards,
Jean-Marc
Hi,
I'm not sure if this is the correct forum but I am seeing this problem on the TMS570 using CCS code generation toold V4.6.3.
I have some code where I want to validate a parameter that is a function pointer. I am getting an "operand types are incompatible" warning message even though the types are the same. Here is an example that highlights the problem:
int test(void);
static void test1(void); static void test2(void);
int test(void)
{
int i = 0;
if(&test1 > &test2) /* Warning on this line */
{
i = 1;
}
return i;
}
static void test1(void) { }
static void test2(void) { }