This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320F28377S: "warning: Data is being written to auto-generated file MyProject.m10" since compiler v17.6

Part Number: TMS320F28377S


Tool/software: TI C/C++ Compiler

Hello

I'm working on CCS v7 with a project using the F28377s

This morning, I have updated the compiler from v17.3 to v17.6.

I have the following warning message at the end of link if the both condition are meet:

- Compiler v17.6

- Properties-> Build -> C2000 Hex utility ->"Enable C2000 Hex utility" ticked.

What does mean this warning? How remove it?

Thank

  • I don't see the diagnostic.  Please perform a complete build, then submit the contents of the Console view (not Problems view).  Use the icon Copy Build Log to save all of the Console view to a file.  Be sure to use the file extension .txt.  Then attach that to your next post.

    Thanks and regards,

    -George

  • Hi

    Please find attached file.

    Warning Log.txt

  • Unfortunately, you have found a bug in the hex utility.  It issues the diagnostic ...

    warning: Data is being written to auto-generated file SMD_Boot_Project.m10
    

    ... even though that file is never created.  As far as I can tell, this is the only error the hex utility makes.  The main hex utility output file is present and correct.  This means the workaround is simple: Just ignore this diagnostic.

    I filed CODEGEN-2372 in the SDOWP system to have this addressed.  You are welcome to follow it with the SDOWP link below in my signature.

    Thanks and regards,

    -George

  • Hi,

    Thank for your back.
    I try to follow the CODEGEN-2372 like you said, but this issue is not found..
    Please, could you verify if you d'ont made a mistake on the number "2372"?
  • It takes a few hours for a new entry to propagate out to the external view.  It should be there soon.  Sorry about that.

    Thanks and regards,

    -George

  • Ok
    Thank for this.
    Have you an idea about the time would take this correction?

    Because one of the safty rules in our project is:
    - Don't have any warning or suspicious message on tool chain (compiler, linker....), else we must made some justifications of this!
  • A GIR said:
    Have you an idea about the time would take this correction?

    For this specific issue, I don't know.  For similar sorts of issues, a fix is available in something around 3 months.

    Thanks and regards,

    -George