Part Number: MSP430FR5969
Tool/software: Code Composer Studio
About energy trace in CCSv7
I am using MSP430FR5969 device.
I was trying to use energy trace tool in code composer studio but I am having trouble using it.
When I start measuring the power consumption of the device, It is only tracking until one second.
As you can see in the picture below, time stamp is moving between 0 to 1. 0->1->0->1...... so the trace is overlapped between 0 to 1.
And also the number the device is measuring seems to have a problem.
Does anybody have an idea for it?
Best,
Mirae