Part Number: TMS320F28035
Tool/software: Code Composer Studio
Hi Sir/Ma'am,
Good Day!
I have been trying to load program at TMS320F28035 using FTDI, but whenever I try to connect the target it gave me error:
C28xx: Error connecting to the target: (Error -151 @ 0x0) One of the FTDI driver functions used during the connect returned bad status or an error. The cause may one or more of: invalid emulator serial number, blank emulator EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the emulator can be located. (Emulation package 5.0.872.0)
I have found an inquiry here with the same problem, and I did applied the suggested action, I download the MPROG and use the application. I also downloaded the XDS100 ept, but as I click the "Devices" at the menubar and try to click among, "scan", "erase', "program", it give me an error of "MPROG.exe has stopped working".
What must I do then?
Thank you