Tool/software: Code Composer Studio
Hello,
I am using Launch Pad to debug MSP430G2553 which is standalone. The TEST, RESET and GROUND pins of Launch Pad are connected to the g2553 chip. When i try to debug the chip with Code Composer Studio (Version: 6.1.1.00022), the error windows in the below appear.
The configuration of the project is:
I can see the MSP430 in the device manager:
Also the device id of the MSP430 is:
Can you please help me to solve this?
Best regards.