Part Number: TMDSEMU110-U
Other Parts Discussed in Thread: UNIFLASH, TM4C129CNCPDT
Tool/software: Code Composer Studio
I'm using the Uniflash GUI and the Standalone command line tool with an XDS110 debug probe, and a TM4C129CNCPDT chip. When I flash new firmware to the board using the debugger and uniflash the board isn't reset upon completion. I have used the same workflow with the XDS200 and after the download completes the board is reset and can continue. However, when I use CCS to debug, flashing is not a problem, board is reset and ready to run code.