This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C5515: Bug in Code Composer Studio

Part Number: TMS320C5515


Tool/software: Code Composer Studio

Hello Ti Community,

I am currently using the CCS v6.1. The SPI register settings differ in TMS320C5515 DSP EVM documentation and CCS.

The Register Settings of SPI-->SPI_CMD2-->CMD in CCS is as follows:

00 -- RSV1

01 -- READ

10 -- RSV2

11 -- WRITE

Whereas, in the documentation of TMS320C5515 SPI User's Guide (Page 29) it is as follows:

00 -- RSV1

01 -- READ

10 -- WRITE

11 -- RSV2

I've checked using both settings and I found out that the settings 10 corresponding to WRITE command works. So the documentation stuff is correct and Register view tab(CCS->View-->Registers) in CCS is incorrect.

Attached are the images to explain the same.

  • Ketan,

    Thank you for reporting this; I will pass this information along to the people responsible to generate this package.

    I will reply back with an estimate on when this will be fixed.

    Please apologize for the inconvenience,
    Rafael