Tool/software: Code Composer Studio
Hello,
currently I'm using Code Composer 7.2 for SimpleLink CC3200 devices (TI v16.9.3.LTS Compiler). As it seems, there is no indexer available. Furthermore, as it seems, the whole "C/C++" section in the Window->Preferences dialog is missing - this is the part of the menu where the indexer should be referenced, like it also was on every other Eclipse-based IDE I have used so far. ;)
I also tried the search field in the Preferences dialog but the word "indexer" brings up nothing.
Apart from that, the IDE seems to work. Project compile, debugging debugs, etc.
Did I miss something? Did I do something wrong on installation? I need indexing for productive use of the IDE. Could anyone tell me how to get it?
Greetings