Part Number: TM4C123GH6PM
Tool/software: Code Composer Studio
1)I am facing the following errors while adding the example project in the workspace. The addition is successful only for blinky.
Error: Import failed for project " hello" because its compiler definition is not available.
I have also tried re-installing it many times. Please solve this issue.
2) I am also facing the following error during compilation of the example codes
Error 1965: Can't open sourcefile "inc/tm4c123gh6pm.h"