This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMDSLCDK138: PC Trace analyzer setup in CCS 7.1.0

Part Number: TMDSLCDK138
Other Parts Discussed in Thread: OMAP-L138

Tool/software: Code Composer Studio

I have been using Trace analyzer with ETB as receiver in CCS 5.3.0 and it works perfect for my need. I recently moved to CCS 7.1.0 and found that trace control has been moved under Hardware Trace Analyzer as PC Trace. When i setup the receiver as ETB and start the trace, it ends with error "Could not run Analyzer on ARM9_0. Cause: Cannot get lock status register id." I ensured that ETB core is connected. Request your help in resolving this. 

Processor: OMAP-L138

Emulator: XDS200 USB emulator.

Thanks,

Chaithanya.