This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CCSTUDIO: MacOS Host Support CCSv7 - Does Does CCS7 for MacOS support J-Link?

Part Number: CCSTUDIO
Other Parts Discussed in Thread: CC3200, CC2640R2F, MSP-FET

Tool/software: Code Composer Studio

Hello, I bought a new MacBook Pro-2016 and I'm planning to install CCS7 to work with projects which use TM4C123, MSP432, CC2640R2F, and CC3200 MCUs.

By the way, from "J-Link - Supported devices";

TM4C123XXXXX

MSP432P4XXX

CC26XXXXX

CC3200

were on the list.


I searched TI's Wiki pages.

1. J-Link Emulator Support: The SEGGER integration feature is now shipped with the CCSv7 install package. The feature is not installed by default and would need to be checked during installation.

2. MacOS Host Support CCSv7, Supported Debug Probes:

MSP-FET430UIF
MSP-FET
ICDI
XDS100v1/XDS100v2/XDS100v3
XDS110
XDS200/XDS220

Hmm, the J-Link was not specified in the Wiki page.

I have both J-Link Edu and J-Link Plus. Are these debug probes supported?

Since they are not written on the Wiki page, I want to double check.