This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC3200-LAUNCHXL: Problems while Installation of CCS

Part Number: CC3200-LAUNCHXL


Tool/software: Code Composer Studio

Hello,

I have just started installation of code composer studio, and my system configuration is Windows 7, SP1, 64 bit. I am facing following errors while installation:

As for the error regarding Windows update I tried to manually download and install the update, but it was unsuccesful because it says the update is already installed. And then if I click on Continue as it is, after a while I see the second error and the installation is not successful. Please help!