Part Number: TMS320C6657
Tool/software: Code Composer Studio
Hello,
I am currently following a user guide to run the demo program for the H.264 decoder software in Code Composer Studio 5 and I am having trouble building the project. To the best of my knowledge, I have followed the guide well. However, two error messages pop out:
Resource Path Location Type
Program "C:/ti/bios_6_33_06_50C:/ti/ccsv5/utils/bin/gmake" is not found in PATH
Resource Path Location Type
Program "C:/ti/bios_6_46_05_55C:/ti/ccsv5/utils/bin/gmake" is not found in PATH
The additional CCS software folders are stored in "C:/ti/", so "C:/ti/bios_6_33_06_50" does exist and "C:/ti/ccsv5/utils/bin/gmake" also exists (I double checked). The file paths mentioned in the error do not make sense to me because they seem to combine the two file paths I just mentioned.
The user guide that I am using told me to download SYS/BIOS version 6.33.06.50, but I have several other SYS/BIOS versions in the same folder. Removing the other SYS/BIOS folders from the same folder do not affect the error messages. Are other folders trying to call the different SYS/BIOS versions?
I would greatly appreciate any assistance on why this error occurred and what this error is telling me to fix?
Thank you,
Joseph