Part Number: TMS320C5505
Other Parts Discussed in Thread: CCSTUDIO
Tool/software: Code Composer Studio
Hi all specialists,
need a bit of help:The configuration is c55xx--bypass_8. This worked for three years now and is used to preload the c5505 before programming via its rs232. ds speed is 1MHz or lower which does not matter.
Running Kubutu 17.04 ( 16.04 the same ). First, CCS stopped working at all due to segfault after kernel update but this problem is gone since the second last update, may be three weeks ago. The comments in ./eclipse/ccsstudio.ini are removed.
Now the xds100v2 cannot connect to the target on both systems any more. Error -1063. There is no answer on TDO, even the nops are not seen whereas TDI Signals are given. Tested on several targets. Even the jtag cable is the same.
Using the MAXIM-jtag-progammer ( bypass_38--isp [win7, virtualbox]) the c5505 does its job and pipes through on the same machine, seen on TDO.
What changed? Any help would be apreciated.
Best,
Frank