This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/66AK2E05: Will Spectrum Digital XDS200 works with K2E processor

Part Number: 66AK2E05

Tool/software: Code Composer Studio

Hello Sir,

We want to use XDS200 with K2E processor on CCSv7.2. 

In CCS when we select the 66AK2E05 device then under debugger section - it mention "TI XDS2xx USB Debug probe". There is no "Spectrum digital and Blackhawk XDS200 USB debug probe listed in that debugger list. i have attached the snapshot for ssupported debugger listed for K2E device in CCS tool.

We have few question regarding this - 

1) if we use "Spectrum Digital XDS200 USB debugger" and select the "TI XDS2xx USB debug probe" in CCS tool. will this settings works? 

2)  if we use "Blackhawk XDS200 USB debugger" and select the "TI XDS2xx USB debug probe" in CCS tool. will this settings works?

3) K2E EVM has an internal XDS200 debugger. is this internal XDS200 debugger same as Spectrum digital XDS200 or Blackhawk XDS200 debugger? 

Please reply as soon as possible. 

Thanks and Regards

Tarang Jindal

  • Hello,

    Tarang Jindal68 said:
    In CCS when we select the 66AK2E05 device then under debugger section - it mention "TI XDS2xx USB Debug probe". There is no "Spectrum digital and Blackhawk XDS200 USB debug probe listed in that debugger list.

    This is because both Spectrum Digital and Blackhawk XDS200 debug probes use the TI XDS200 drivers. So you would use the "TI XDS2xx USB Debug probe" option for all XDS200 USB probes regardless of vendor

    Tarang Jindal68 said:
    1) if we use "Spectrum Digital XDS200 USB debugger" and select the "TI XDS2xx USB debug probe" in CCS tool. will this settings works? 

    Yes

    Tarang Jindal68 said:
    2)  if we use "Blackhawk XDS200 USB debugger" and select the "TI XDS2xx USB debug probe" in CCS tool. will this settings works?

    Yes

    Tarang Jindal68 said:
    3) K2E EVM has an internal XDS200 debugger. is this internal XDS200 debugger same as Spectrum digital XDS200 or Blackhawk XDS200 debugger? 

    It is similar HW but you would use the "TI XDS2xx USB Onboard debug probe" option in the connection selection list 

    Thanks

    ki