This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/CC430F5137: Communication issue above 4kb programmable flash memory.

Part Number: CC430F5137

Tool/software: TI C/C++ Compiler

Dear All,

I am working CC430F5137 and facing the issue of communication after programming flash memory goes above 4 Kb, my another function is working alright.

Please give me the solution.

Thanks in advance.

Regards,

Avinash T.

  • Avinash,

    Please provide more details about what issues you are seeing. I recommend making a simplified software example that can represent your issue such that we can replicate the issue in our labs.

    Regards,
    /TA
  • Thank you for your valuable reply. Actually my application's code is very small 5992 Kb, even though CC430F5137 is having 32Kb programmable flash memory.

    Whenever I extend the code size, above 4 Kb then its communication will stop with paired device but the remaining functions are very working fine in both cases and when code size is increases above 4 kb then i observed that output its frequency change from 868MHz to  860Mhz.

    Please give a solution.

    Thanks In Advance

  • Thank you for your valuable reply. Actually my application's code is very small i.e. 5.992 Kb, even though CC430F5137 is having 32Kb programmable flash memory.

    Whenever I extend the code size, above 4 Kb then its communication will stop with paired device but the remaining functions are very working fine in both cases and when code size is increases above 4 kb then i observed that its frequency change from 868MHz to 860Mhz.

    Please give a solution.

    Thanks In Advance