This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler: Measuring tank width should ?

Other Parts Discussed in Thread: TDC1000, TDC7200

Tool/software: TI C/C++ Compiler

Hello, 

i have worked on TDC1000 & TDC7200 for level measurement. I done with it. but when i change tank it is not working even with TDC1000-TDC7200EVM GUI interface. Same sensor i used for plastic results exactly but for thick tanks its not working properly.

Thanking You

  • Hi Kishore,

    This is most likely due to poor coupling between the trasnducer and the tank. Please reference the following application note for proper mounting instructions: www.ti.com/.../snaa266a.pdf

    Additionally, for very large tanks it may be a good idea to use a focus tube to help with the signal integrity and stabilize the level when tilted. This is just a tube with a small hole in the bottom that is attached inside the tank directly where the trasnducer is located on the outside.

    Regards,