Part Number: TMS320F28375D
Other Parts Discussed in Thread: UNIFLASH, CCSTUDIO
Tool/software: Code Composer Studio
Hello,
I'm using Ubuntu 14.04 on a dell server machine.
Linux itws005 4.2.0-42-generic #49~14.04.1-Ubuntu SMP Wed Jun 29 20:22:11 UTC 2016 x86_64 x86_64 x86_64 GNU/Linux
I downloaded CCS v7 just last week, so it should be a recent version.
When I go to open the debugger to flash the built image to the device, it has a JRE crash.
I've put the console output below, and attached the error log that is generated.
BTW, We're using CCS7 to attempt to program the flash because UniFlash is not working either. :(
thanks
Jerry
jmorrow@itws005:/opt/ti/ccsv7/eclipse$ ./ccstudio
Aug 03, 2017 5:05:24 PM org.apache.http.impl.client.DefaultRequestDirector tryExecute
INFO: I/O exception (org.apache.http.NoHttpResponseException) caught when processing request to {}->http://link.ti.com: The target server failed to respond
Aug 03, 2017 5:05:24 PM org.apache.http.impl.client.DefaultRequestDirector tryExecute
INFO: Retrying request to {}->http://link.ti.com
Aug 03, 2017 5:05:24 PM org.apache.http.impl.client.DefaultRequestDirector tryExecute
INFO: I/O exception (org.apache.http.NoHttpResponseException) caught when processing request to {}->http://link.ti.com: The target server failed to respond
Aug 03, 2017 5:05:24 PM org.apache.http.impl.client.DefaultRequestDirector tryExecute
INFO: Retrying request to {}->http://link.ti.com
Aug 03, 2017 5:05:24 PM org.apache.http.impl.client.DefaultRequestDirector tryExecute
INFO: I/O exception (org.apache.http.NoHttpResponseException) caught when processing request to {}->http://link.ti.com: The target server failed to respond
Aug 03, 2017 5:05:24 PM org.apache.http.impl.client.DefaultRequestDirector tryExecute
INFO: Retrying request to {}->http://link.ti.com
agent.js is not found at /opt/ti/ccsv7/ccs_base/cloudagent/server/public.
dvtLogOptions.xml DOES NOT exists
#
# A fatal error has been detected by the Java Runtime Environment:
#
# SIGSEGV (0xb) at pc=0x00007f565261f917, pid=2513, tid=0x00007f553cff5700
#
# JRE version: Java(TM) SE Runtime Environment (8.0_112-b15) (build 1.8.0_112-b15)
# Java VM: Java HotSpot(TM) 64-Bit Server VM (25.112-b15 mixed mode linux-amd64 compressed oops)
# Problematic frame:
# C [libDebugServer.so+0x549917]
#
# Failed to write core dump. Core dumps have been disabled. To enable core dumping, try "ulimit -c unlimited" before starting Java again
#
# An error report file with more information is saved as:
# /tmp/hs_err_pid2513.log
#
# If you would like to submit a bug report, please visit:
# bugreport.java.com/.../crash.jsp
# The crash happened outside the Java Virtual Machine in native code.
# See problematic frame for where to report the bug.
#
Aborted (core dumped)
hs_err_pid2513.log