This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C28346: CCS 7.2.0 update RTOS analyzer disappears after initialize

Part Number: TMS320C28346


Tool/software: Code Composer Studio

Hello,

I updated yesterday from 7.1 to 7.2, and also installed the other updates like the compiler from 16.9.3 to 16.9.4

afterwards I updated the project properties to use the new compiler, and XDCtools 3.50.2.20.

(other settings are SYS/BIOS 6.50.1.12, UIA 2.20.0.02)

But now I can't use the RTOS analyzer anymore.

In 7.1 it took a while to initialize. In 7.2 the initialize goes a lot faster but will disappear in menu after the initialization

The other analyzers have the same issue now.

Any tips to get this working again?