I´m sorry if this is a simple question, but after an hour of searching I have not found a solution,
My PC is configured with both Administrator and User accounts.
The Users have no write access to the D: System drive, which contains the "Windows" and "Program Files" directories. They do however have full access to their part of the C: Documents and Settings directory.
As configured normally, CC has been installed under D:\Program Files. However it will not run in "User" mode as it requires write access to this directory in order to write mew files into \ccsv4\DebugServer\ etc.
Is there a solution to this?
Many thanks
Nicholas Lusty