This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/F28M36H33B2: Create a single CCS Project with 2 processor families

Part Number: F28M36H33B2


Tool/software: Code Composer Studio

Hello,

(NOTE: Please ignore the part number as this question is related to a new device under development)

I am trying to create single CCS project with 2 processor families (ARM and C28). Intention is to have 2 Build Configurations - one for C28 and once for ARM which would pick the appropriate files / build settings  etc to generate the .out.

I have tried several different ways but seems like "Family" tab in Create CCS project pop up gets frozen to 1 family.

Any thoughts?

Thank you and Best Regards,

  • Hello,

    kjk said:
    I have tried several different ways but seems like "Family" tab in Create CCS project pop up gets frozen to 1 family.

    Yes, you are correct. You will need to work with 2 separate projects in your described scenario.

    Thanks

    ki

  • Thanks Lee,

    was kind of expecting that answer. can this be requested as s future CCS feature. Every Project setting in CCS is tied to Build Configuration (except family), unless there is a strong reason "Family" should also be Build Configuration dependent.

    OR is there anything that I am missing.

    Regards,
    -Prashanth JayaPrakash
  • Prashanth,
    Your request is certainly a reasonable one. But because of the way the project system is designed, it will be a difficult one to implement. We will keep it in mind for the future however and perhaps it can be something we can add down the road.

    Thanks
    ki
  • Thanks Lee,

    hope to see it added in the near future.

    Best Regards,

    -Prashanth JayaPrakash