This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430G2553: Installation Failed

Part Number: MSP430G2553

Tool/software: Code Composer Studio

Hello!

I was trying to install CCS and I made sure to turn off my anti-virus. I had the following error:

I will also attach the install log files.

20170809123952.rar

Any help would be appreciated.

  • I see in your install logs that your system TEMP directory is set to a directory that has spaces in it (which is coming from your Username that has a space between two names). There is a known issue with the CCS installer when there are spaces in the Windows temporary directory path. During the install, we extract files to the TEMP directory but this step fails if the TEMP directory has spaces in the path.

    Please see this post for a workaround.

    This issue will be fixed in the next CCS release 7.3.